earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-P-3, AS-B, Device Administrator, AS-P
Functionalities: Security
Product version: 7.0, 7.1
8/31/2026

Configuring an Automation Server to use 802.1X EAP TLS Security

You configure an automation server to use 802.1X EAP TLS to increase the security.

Show More
action_close

Automation servers support IEEE 802.1X security. Automation servers can be configured as supplicants on a network protected by IEEE 802.1X security.

The following IEEE 802.1X authentication methods are supported:

  • MD5

  • EAP TLS

  • Protected EAP with MSCHAPv2

Important:

When using IEEE 802.1X Security, Ethernet 2 cannot be set to switch mode.

To configure an automation server to use 802.1X EAP TLS security
  1. Connect to the USB device port. For more information, see Connecting to an Automation Server Using the USB Device Port .

  2. In Device Administrator, click Servers and then click the server name.

  3. Click 802.1X Security .

  4. In the 802.1X Security list, select EAP TLS .

  5. In the Identity box, type the identity as configured on the authentication server.

  6. In the CA Certificate box, browse to the CA certificate.

  7. In the Client Certificate box, browse to the client certificate.

  8. In the Private key box, browse to the private key associated with the client certificate.

  9. In the Private key password box, enter the private key password.

  • Security Overview
  • IEEE 802.1X Security
  • Field Server Administration Overview
  • 802.1X Security – EAP TLS Tab
  • Connecting to an Automation Server Using the USB Device Port