Use the Appearance tab to configure user settings such as language, time, and display mode.
Component |
Description |
Show invalid objects |
Select if the user should be able to see invalid objects. For more information, see Invalid Objects . |
Enable session notification |
Select if the user should be able to enable session notifications. |
Only use classic function block program user |
Select if the user only can use classic function block program. For more information, see Graphical Programming . |
Language |
Select the user’s language. For more information, see Regional Settings . |
Date, time and number format |
Select the user’s date, time, and number format. For more information, see Regional Settings . |
System of measurement |
Select the user’s system of measurement. For more information, see Regional Settings . |
Decimals |
Select the user’s decimals. For more information, see Regional Settings . |
Relative time |
Select the user’s relative time. For more information, see Regional Settings . |
Dark Mode |
Select the user’s dark mode. For more information, see Theme Settings . |
Size Mode |
Select the user’s size mode. For more information, see Theme Settings . |
Workspace Layout |
Select the user’s workspace. |