Log on to rate and give feedback    1 2 3 4 5 Log on to rate
0
Troubleshooting Troubleshooting 11/18/2022
Products: AS-B, AS-P, Project Configuration Tool
Functionalities: b3
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022

b3 BACnet Object Copy and Paste Errors

Copying and pasting a group of b3 BACnet objects results in a Duplicate BACnet name or Unknown object alarm.

Solution

Copy and paste BACnet objects and folders with WorkStation in database mode and then execute a Download all objects command to download pasted objects. The download resolves the errors.

For more information, see Database Mode .

For more information, see Downloading to a b3 BACnet Device .

Community Content

Product version

Language