Add and Configure Alarms Using WebStation
You can add and configure alarms using WebStation.
Alarms can be created from a value using WebStation.
For more information, see Creating an Alarm from a Value in WebStation
.
You can click on an alarm using WebStation to open the properties of the alarm for editing.
A special feature, only available when using WebStation, is displaying alarm limits in trend charts.
For more information, see Display Alarm Limits in a Trend Chart in WebStation
.
Creating an Alarm from a Value in WebStation
Display Alarm Limits in a Trend Chart in WebStation
Change of State Alarm Trigger Properties
Enumeration Alarm Trigger Properties
Matching Text String Alarm Trigger Properties
Multistate Alarm Trigger Properties
Out of Range Alarm Trigger Properties
Out of Reference Range Alarm Trigger Properties
Sum Alarm Trigger Properties
Variable Status Alarm Trigger Properties
Alarm Attachments Dialog Box
User Actions Dialog Box
Alarm Presentation Dialog Box