earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Security
Product version: 7.0, 7.1
10/30/2025

Certificates Managed Using WorkStation

Certificates are used to increase the security of the communication between EBO servers and clients like WorkStation and WebStation.

WorkStation certificate workflow

Use this workflow to generate and activate a self-signed certificate using WorkStation.

For more information, see WorkStation Generate Certificate Workflow .

Use this workflow to purchase, convert and install CA server certificates using WorkStation.

For more information, see WorkStation Server CA Certificate Workflow .

Checking the status of a certificate using WorkStation or WebStation

For more information, see Checking the Status of the Certificate Using WorkStation or WebStation .

Remove certificates

You can remove a certificate using WorkStation

For more information, see Removing a Certificate Using WorkStation .

Windows Certificate Store for Enterprise Server and Enterprise Central

You can use Windows Certificate Store to store certificates used for Enterprise Server and Enterprise Central authentication. In this case you do not use WorkStation for the storage functions. Instead you use Certmgr.exe, Windows Certificate Manager Tool.

For more information, see Windows Certificate Store for Enterprise Server and Enterprise Central .

  • Certificates
  • WorkStation Server CA Certificate Workflow
  • WorkStation Generate Certificate Workflow
  • Checking the Status of the Certificate Using WorkStation or WebStation
  • Removing a Certificate Using WorkStation
  • Windows Certificate Store for Enterprise Server and Enterprise Central