Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
You add a calendar exception to apply an exception event for all dates specified in the calendar.
In Operator Display, on the Device List screen, tap the arrow button
On the Device screen, tap the Schedules arrow button
On the Schedules screen, tap the schedule to which you want to add a date range exception event.
On the schedule view screen, tap the add event button
On the Add schedule event screen, tap Calendar exception .
If the Calendar exception button is gray instead of blue, and you see No calendars found next to it, this option is unavaible for the moment on this device because at least 1 configured calendar is required.
On the Add calendar exception screen, in the Priority box, tap + or - to edit the priority of the event.
1 is the highest priority and 16 is the lowest.
Next to the Calendar box, tap on the pencil button
On the Select calendar screen, tap the radio button next the calendar you want to edit.
Tap OK .
On the start/end time and value list header, tap the add time span and value button
On the Edit exception event screen, select the event value:
For analog, multi-state and enumerated schedules: In the Value box, tap + or - to specify the value of the event.
For digital schedules: Tap Inactive or Active (Off or On).
Select the time span type:
Tap All day to make the event span 24 hours.
In the From and To boxes: tap + or - to select the starting and ending times.
Tap OK .
You can add multiple time spans and values to an exception event.
On the Add calendar exception screen, tap OK .
On the schedule view screen, tap Save .