earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebStation
Functionalities: Basic Functionality
Product version: 2024, 7.0
10/30/2025

Navigate from Path

You can navigate from a path using WebStation. This is useful for example if you want to inspect or make changes to a value that is monitored by an alarm. In this case you open the properties dialog box for the alarm, right click on the value in the path in the Monitored variable field, and right-click and click Open or pen in a floating window.

The value you can navigate to turns blue when you hover over it.

The navigation from path is also available in a search result list.

  • Navigating from Path