earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Sustainability
Product version: 7.0
7/2/2025

Reset a Meter Object

Meter objects can be reset. This is typically done after you have tested a meter object configuration or when you want to restart the calculation and logging in a meter object.

When you reset the meter object, the meter object log is cleared and the calculated consumption is set to 0. The meter object then restart calculation and logging.

You can reset multiple meter objects at the same time using Search and mass editing.

For more information, see Search Overview .

For more information, see Mass Editing Objects .

  • Meter Object
  • Resetting a Meter Object