Use the XLSX Report – Basic tab to configure the XLSX report.
Component |
Description |
Enabled |
Select to enable the XLSX report. |
Sending notification |
Select to enable the sending of the XSLSX report. |
![]() |
Add Click to add a write to file. |
![]() |
Edit Click to configure write to file. For more information, see Create Object Wizard - Configure Write to File Page . |
![]() |
Remove Click to remove a write to file. |
![]() |
Add Click to add an email recipient. |
![]() |
Edit Click to configure an email recipient. For more information, see Create Object Wizard - Configure Email Page . |
![]() |
Remove Click to remove an email recipient. |
Time range |
Select the time range for the XLSX report. |
Time period |
Select the time period. |
Fetch delay |
Select the waiting time before the XLSX report is written or sent. |
Alarm activation schedule |
Enter the schedule that contains the value that activates the XLSX report. |
Schedule value when active |
Enter the value, generated by the connected schedule or other multistate variable, that activates the XLSX report. |
Custom time range type |
Select time span or span range for the XLSX report. |
Custom time span |
Enter a time span for the XLSX report. |
Custom start time |
Enter a start time. |
Custom end time |
Enter a end time |
Time zone |
Select the time zone. |
Localization |
Select a language among the language packs installed on the EcoStruxure BMS server. |
System of measurement |
Select the system of measurements to be used in the XLSX report. |
Timepstamp format |
Type the format of date and time that you want to use in the XLSX report. |
Decimal count |
Select the number of decimals you want to include in the XLSX report. |
Decimal symbol |
Select the decimal symbol to be used in the XLSX report and the XLSX report template. |
First day of week |
Select the day to be set as the first day of week. |
Sort order |
Select the sort order used in the XLSX report. |
Substitution missing data with |
Enter the text that is displayed when a value is missing. By default, a missing value display nothing at all. |
Trigger variable |
Enter the variable that triggers the XLSX report. |
Trigger condition |
Select when you want the XLSX report to be triggered: when the trigger variable changes to true, changes to false, or all changes. |