earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2024, 7.0
12/10/2024

XLSX Report Template Tab

Use the XLSX Report Template tab to create, edit, and load a template.

 
action_zoom_plus_stroke XLSX Report Template Tab
Figure: XLSX Report Template Tab

Table: XLSX Report Template Tab

Component

Description

Load Template

Click to load a custom type template. For more information, see Custom Types Overview .

Create Template

Click to create a template. Only available when no template has been created. For more information, see XLSX Template Tab .

Edit template

Click to open the XLSX template tab. Only available when a template has been created. For more information, see XLSX Template Tab .

Generate preview

Preview generated report

Click to preview a generated report including all data.

Preview generated report without data

Click to preview the substitution codes without any data. Use this preview to make sure that the context does not overlap.

Current template

Displays the name for the template in use.

  • XLSX Reports Overview
  • XLSX Reports Workflow
  • XLSX Report Template Tab
  • XLSX Template Tab
  • Custom Types Overview
  • Context Configuration – Template Tab
  • Context Configuration – Calculation Tab
  • Context Configuration – Misc Tab