earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Localization
Product version: 7.0
12/19/2024

Displaying the Local Time for a Server in the Time Stamp Value Object

You display the server time using a Time Stamp Value object when you want to display the local time for a server in another time zone than the client time zone.

Show More
action_close

You can present the server time zone in, for example, graphics or notifications, using the Time Stamp Value object. The time can be displayed in the server time zone and not in the client time zone.

For example, you have one server in New York and one in London. You supervise both from your location i Stockholm using WorkStation. The server time in New York and London are displayed locally in your time zone but you want the server in New York to display the time in New York and the server in London to display the time in London. In this case configure a Time Stamp Value to display the local server time in WorkStation.

For more information, see Displaying the Local Time for a Server in the Time Stamp Value Object .

To display the local time for a server in the Time Stamp Value object
  1. In WorkStation, in the System Tree pane, select the folder or EcoStruxure BMS server where you want to create the Time Stamp Value.

  2. On the File menu, point to New object , select Time Stamp Value and click Create .

  3. Open the Time Stamp Value objects properties.

  4. In the properties dialog, in the Value field, click the Configure button

     
    action_zoom_plus_stroke
    .

  5. In the Value dialog box, click the Configuration tab.

  6. In the Reference field, browse to the server you want to display the time for.

  7. Browse to the server and select Server time .

  8. Click Select .

  9. Click OK .

  10. In the Localization list, select Server time zone .

  11. Click Save .

The local server stamp time is now displayed in the Formatted timestamp field.

  • Display Server Time
  • Time Stamp Value Properties