You can present the server time zone in, for example, graphics or notifications, using the Time Stamp Value object. The time can be displayed in the server time zone and not in the client time zone.
For example, you have one server in New York and one in London. You supervise both from your location i Stockholm using WorkStation. The server time in New York and London are displayed locally in your time zone but you want the server in New York to display the time in New York and the server in London to display the time in London. In this case configure a Time Stamp Value to display the local server time in WorkStation.
For more information, see Displaying the Local Time for a Server in the Time Stamp Value Object .