earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: BACnet, Engineering, Touchscreen Room Controller
Product version: 2024
6/27/2024

Select Firmware Dialog Box

Use the Select Firmware dialog box to select the Touchscreen Room Controller firmware version from the list. All Touchscreen Room Controller firmware upgrade files have the extension .trcfw.

 
action_zoom_plus_stroke Touchscreen Room Controller Select Firmware dialog box
Figure: Touchscreen Room Controller Select Firmware dialog box

Table: Touchscreen Room Controller Select Firmware Dialog Box

Component

Description

Firmware

Displays a list of Touchscreen Room Controller firmware versions available on the EBO server.

Name

Displays the name of a Touchscreen Room Controller firmware version.

Firmware version

Displays the version string of a Touchscreen Room Controller firmware version.

Download firmware

Select the Download Firmware checkbox to download the firmware version to the selected Touchscreen Room Controller.

Activation Immediately

Select to upgrade the Touchscreen Room Controllers immediately after firmware file transfer.

Activation Time

Select to schedule the upgrade for a later time. Specify the date and time when you want the upgrade to take place. Be sure to allow enough time for the firmware to be transferred to all of the selected Touchscreen Room Controllers.

OK

Click OK to begin upgrading the selected Touchscreen Room Controllers.

Cancel

Click Cancel to exit the Select Firmware dialog without upgrading the Touchscreen Room Controllers.