Use the Advanced tab to view the properties of the Touchscreen Room Controller upgrade package.
Property |
Description |
Object ID |
Displays the BACnet object type and instance number of the object. |
BACnet name |
Indicates the BACnet name of the object. |
BACnet type |
Indicates the BACnet type of the object. |
Profile name |
Displays the unique name of the profile that describes the characteristics of the object, such as additional properties, behaviors, or requirements.
|
Apply upgrade |
Used during firmware upgrade. |
Name |
Used during firmware upgrade. |