The EcoStruxure Building Operation software includes programing tools for server and controller programming and dynamic graphics programming. Some of the tools are integrated in WorkStation and some are external applications. You choose which of the external applications you want to install during the WorkStation installation.
You can use Graphics Editor to create and edit graphics representing a site and the devices that make up the site.
For more information, see Graphics Editor .
Visual programming in Builder for Function Block allows users of EcoStruxure BMS to create, edit and configure Function Block programs that control and monitor building automation systems by manipulating program elements graphically instead of specifying them textually.
For more information, see Builder for Function Block Overview .
Function Block Editor is a graphical programming tool for EcoStruxure BMS servers and MP controllers, which you use to create function block programs that control and monitor building automation systems. For example, you create a basic program, called OfficeLight, to control lighting in a room based on occupancy.
For more information, see Function Block Editor Overview .
Script programs are text-based instructions that tell the EcoStruxure BMS server to take some kind of action to control a building.
For more information, see Script Overview .