There are three LEDs on the front of the Twisted Pair Adapter. The LEDs indicate different types of status and modes.
|
Function |
Color |
|
NET Link |
Green/Red a |
|
Ethernet |
Green/Red a |
|
Master |
Green/Red a |
The LEDs indicate the status of the device, the status of the connections to the twisted pair cable network (NET) and Ethernet (LAN), and which operating mode the device is configured for.
The NET Link LED indicates the status of the device's connection to the twisted pair cable network (NET).
|
LED Patterns |
Condition |
Recommended Action |
|
Red, constant |
Detected error, attention required. |
Contact Schneider Electric Product Support Services for assistance or return the device to Schneider Electric. |
|
Green, constant |
Normal operation. Connection to the twisted pair cable network (NET) is established. |
No action required. |
|
Green, flashing |
The device is initializing after pressing the INIT button for 2 seconds. Wait until the initialization is complete. Initialization restarts the device. |
No action required. |
|
No light |
The device is operating normally but has not established a connection to the Master device on the twisted pair cable network (NET). |
Connect the twisted pair cable. |
|
No light |
No input power. |
Connect 24 VAC 50/60 Hz or 24-30 VDC. |
The Ethernet LED indicates the status of the device's Ethernet (LAN) connection and the data communication activity on the link.
|
LED Patterns |
Condition |
Recommended Action |
|
Red, constant |
Detected error, attention required. |
Contact Schneider Electric Product Support Services for assistance or return the device to Schneider Electric. |
|
Green, constant |
Normal operation. An Ethernet (LAN) cable is connected to the device. |
No action required. |
|
Green, flashing |
Normal operation. The device is transmitting and receiving data. |
No action required. |
|
Green, flashing |
The device is initializing after pressing the INIT button for 2 seconds. Wait until the initialization is complete. Initialization restarts the device. |
No action required. |
|
Amber, constant |
No Ethernet link detected. |
Plug in the Ethernet cable and turn on the connected device. |
|
No light |
No input power. |
Connect 24 VAC 50/60 Hz or 24-30 VDC. |
The Master LED indicates whether the device is configured in Master mode (when connected to an automation server) or Terminal mode (when connected to a SpaceLogic BACnet/IP controller).
|
LED Patterns |
Condition |
Recommended Action |
|
Green |
Normal operation. The device is in Master mode after moving the Master/Terminal (M/T) switch to the M position. |
No action required. |
|
Green, flashing |
The device is initializing after pressing the INIT button for 2 seconds. Wait until the initialization is complete. Initialization restarts the device. |
No action required. |
|
No light |
Normal operation. The device is in Terminal mode after moving the Master/Terminal (M/T) switch to the T position. |
No action required. |
|
No light |
No input power. |
Connect 24 VAC 50/60 Hz or 24-30 VDC. |