earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Commission
Functionalities: Security
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0, 7.1
4/28/2026

EcoStruxure Building Commission

These hardening guidelines apply to the EcoStruxure Building Commission mobile application.

Exploit Protection Mitigation

On all devices running Microsoft Windows where Commission mobile application is installed:

  • Ensure that exploit protection mitigation is enabled on the computer.

  • Ensure that Export Address Filtering (EAF) is enabled for SE.EBC.exe.

    • If supported, ensure to validate access for modules that are commonly abused by exploits.

For more information, see Microsoft Learn – Exploit protection

In addition:

  • Review and align additional exploit protection mitigations with your internal endpoint hardening standards.

  • Test the setting in a representative environment before broad deployment, especially if additional exploit protection rules are enabled.

  • Document the applied configuration as part of the site hardening baseline and change management process.