earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Enterprise Server, AS-P, Virtual Project Servers
Functionalities: LonWorks, Xenta
Product version: 2024
5/26/2025

Actions Menu – Advanced Commands Submenu

Use the Advanced Commands submenu to execute functions on the selected LonWorks device or Xenta device.

 
action_zoom_plus_stroke Actions menu - Advanced commands submenu
Figure: Actions menu - Advanced commands submenu

Table: Advanced Commands Submenu

Command

Description

Wink

Click to generate a response from the device, such as flashing the power LED.

Clear Status

Click to clear the diagnostic data for the device or local node. For more information, see LonWorks Device Properties – Diagnostics Tab .

Warm Start

Click to restart the device without clearing the RAM memory. For more information, see Xenta LonWorks Device Restart .

Cold Start

Click to restart the device and clear the RAM memory. For more information, see Xenta LonWorks Device Restart .

Alarm Refresh

Click to transfer all alarms buffered in the physical Xenta device to the EcoStruxure Building Operation database. For more information, see Alarms for Xenta LonWorks Devices .

  • LonWorks Device Properties – Diagnostics Tab
  • Xenta LonWorks Device Restart
  • Alarms for Xenta LonWorks Devices
  • Xenta LonWorks Groups