Log on to rate and give feedback    1 2 3 4 5 Log on to rate
0
How to How to 1/4/2011
Products: WorkStation
Functionalities: Schedules
Product version: 1.0, 1.1, 1.2, 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022

Adding a New Event to a Schedule

You add a new event to a weekly schedule using the Basic Schedule Editor.

To add a new event to a schedule
  1. In WorkStation, click the schedule with the event you want to change.

  2. In Basic Schedule Editor, click the View weekly schedule events button .

  3. Click on the schedule where you want to add the new event.

  4. Drag the pointer over the area where you want to create the new event.

  5. On the File menu, click Save .

Community Content

Product version

Language