earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WorkStation, WebStation
Functionalities: Basic Functionality, Graphics
Product version: 2024, 7.0, 7.1
10/30/2025

Changing a Value in a Graphic

You change a value in a graphic when you want a different value.

Show More
action_close

You use graphics to display building overviews, display the status of detectors and alarms, display the value of sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.

A graphic that contain links to documents, such as Microsoft Word or Adobe PDF, can be opened in WorkStation and WebStation. The associated programs, in this case Microsoft Word or Adobe Reader, has to be installed on the computer running WorkStation or WebStation.

 
action_zoom_plus_stroke A Graphic with links and interactive components like gauges in WorkStation
Figure: A Graphic with links and interactive components like gauges in WorkStation

Show More
action_close

You use graphics to display building overviews, display the status of detectors and alarms, display the value of sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.

A graphic that contains links to documents, such as Microsoft Word or Adobe PDF, can be opened in WorkStation and WebStation. The associated programs, in this case Microsoft Word or Adobe Reader, have to be installed on the computer running WorkStation or WebStation.

 
action_zoom_plus_stroke A graphic with links and interactive components in WebStation
Figure: A graphic with links and interactive components in WebStation

EcoStruxure Fire Operation has built-in fire graphics that display and interact with the fire detection system. The following information describes how fire graphics works.

Important:

The fire graphic descriptions does not apply if your EcoStruxure Fire Operation configuration has customized graphics instead of built-in fire graphics.

 
action_zoom_plus_stroke Example of a built-in fire graphic in WebStation
Figure: Example of a built-in fire graphic in WebStation

Fire Graphic Headers

If a default graphic is defined in the fire detection system configuration, the Home button

 
action_zoom_plus_stroke
in the fire graphic header displays the default graphic.

If a navigation menu is created in the fire detection system configuration, the Navigation button

 
action_zoom_plus_stroke
in the fire graphic header displays the navigation menu.

Fire Graphic Menus

The graphic menus in EcoStruxure Fire Operation are used to display alarms and alerts in a graphic. The menus are also used to execute commands on loop devices and zones, or on the fire detection system.

For more information, see Fire Graphic Menus .

Sets of Icons in Fire Graphics

There are three sets of icons in fire graphics: default icons, Swedish icons, and Finnish icons. In Fire Expert Graphics manager, you choose which icon set you want the graphics to use.

For more information, see Sets of Icons in Fire Graphics .

To change a value in a graphic
  1. In WorkStation or WebStation, click the graphic with the value you want to change.

  2. Click the value you want to change.

  3. In the Edit properties dialog box, enter the new value.

  4. Click OK .

  • How Graphics Work in Building Operation
  • How Graphics Work in Fire Operation
  • Forced Values
  • Graphics Toolbar
  • Object Property Dialog Box
  • Forcing a Value
  • Forcing a Value
  • Releasing a Forced Value
  • Releasing a Forced Value