earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: ​License Administrator, ​License Server
Functionalities: License Management
Product version: 2.0, 2.1, 3.0, 3.1
2/3/2020

Changing the Flexnet lmadmin License Server Manager Port Number

You change the port number of the Flexnet lmadmin License Server Manager if the default port 8888 is dedicated to other application or blocked by your firewall.

Show More
action_close

The License Server can be managed through a web-based administration tool called FLEXnet License Administrator. You use the Administration part of the tool to view system information and administer License Server user accounts, alerts, and other configuration.

The FLEXnet License Administrator web page is hosted by the License Server. You use a web browser to connect to the web page via HTTP or HTTPS. The default protocol is HTTP through port 8888, that is on the License Server host itself: http://localhost:8888. The default user name is "admin" and the default password is "admin".

The Flexnet License Administrator has two main parts: Dashboard and Administration. Use the Dashboard to view the status and information of the licenses that are activated on the License Server. Alerts, such as status and expiring licenses, are reported in the Alert pane.

 
action_zoom_plus_stroke FLEXnet License Administrator, Dashboard part.

FLEXnet License Administrator, Dashboard part.

Use the Administrator part to view the System information and administer Flexnet License Administrator user accounts, alerts, License Server configuration, or vendor daemon configuration.

 
action_zoom_plus_stroke FLEXnet License Administrator, Administration part.

FLEXnet License Administrator, Administration part.

For more information about FLEXnet License Administrator, click the FLEXnet License Administrator Help button

 
action_zoom_plus_stroke
.

License Server Port Number

With a default installation, the License Server port range is set to 27000-27009. A valid number is any unused port between 0 and 64000.

 
action_zoom_plus_stroke FLEXnet License Administrator, License Server Configuration

FLEXnet License Administrator, License Server Configuration

If the License Server uses other ports than the default port range 27000-27009, the port has to be added in front of the @ in the License Server address on the WorkStation, Enterprise Server, or Client tools.

For more information, click FLEXnet License Administrator Help button

 
action_zoom_plus_stroke
.

FLEXnet License Administrator Port Number

The port number to the FLEXnet License Administrator is configured in the file “server.xml” located on the License Server. The path to the file is: C:\Program Files\Schneider Electric EcoStruxure\Building Operation x.y\License Server\conf, where x.y is the version number. The “port” attribute is found within the “webServer” tag.

 
action_zoom_plus_stroke The port attribute is embedded in the “webServer” tag.

The port attribute is embedded in the “webServer” tag.

To change the Flexnet lmadmin License Server Manager port number
  1. On the License Server, open the folder C:\ProgramData\Schneider Electric EcoStruxure\Building Operation x.y\License Server\conf , where x.y is the version number.

  2. Open the file server.xml with Notepad or other text or code editor.

  3. In the Port attribute within the webServer tag, type the number to an available port.

     
    action_zoom_plus_stroke
  4. Save the file and close the editor.

  5. Restart the License Server.

To access the Flexnet lmadmin License Server Manager, open a web browser and type in the address to the License Server with the new port number.

  • Restarting the License Server
  • Accessing Flexnet lmadmin
  • Flexnet License Administrator, License Server Manager
  • Cannot Access lmadmin, License Server Manager