earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Schedules
Product version: 2023
12/17/2022

Edit Exception Dialog Box

Use the Edit Exception dialog box to add or edit an exception event in the Advanced Schedule Editor.

 
action_zoom_plus_stroke Edit Exception dialog box

Edit Exception dialog box

Table: Edit Exception Dialog Box

Component

Description

Exception name

Type a name for the exception event.

Exception priority

Select a priority for the exception event. Valid values are from 1-16, 1 being the highest priority.

Period type

Select a time category to associate with the schedule event.

Period object

Enter the event associated with the period type.

  • Exception Events in WorkStation
  • General Information Properties – Basic Tab
  • References Tab
  • BACnet Schedules
  • BACnet Prerevision 4 Schedule Properties - Exception Event