You edit a backup rule on an EcoStruxure BMS server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another EcoStruxure BMS server.
In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.
Click the Control Panel tab.
Click Backup rules.
In the Backup rules view, select a backup rule and then click the Edit backup rule button
In the Backup rule dialog box, in the Backup set description box, type or modify the backup comment.
In the Backup content box, change the type of data you want to back up:
Select Configuration only to back up the configuration database and custom object type data. For example, use this option to restore data to a replaced EcoStruxure BMS server with the same name in the system.
Select All data to back up the configuration, historical, and custom object type data. For example, use this option to preserve the configuration and historical data for a specified date and time.
In the Lead rule box, enter a backup rule that references a lead schedule managed on another EcoStruxure BMS server.
In the Enabled box, select Yes to enable the backup rule.
Click OK.
On the File menu, click Save.