After licenses are activated on the License Server, you configure the Enterprise Server connection to the License Server. The address to the License Server is defined during the installation of Enterprise Server using License Administrator.
Number |
Description |
1 |
Configure the Enterprise Server address to the License Server. |
2 |
Remove any demo licenses. |
3 |
When the Enterprise Server starts, it automatically activates an EcoStruxure Building Operation software license. |
If the Enterprise Server does not start, refer to the Enterprise Server log for more information. For more information, see Viewing the Enterprise Server or Enterprise Central System Log .