Log on to rate and give feedback    1 2 3 4 5 Log on to rate
0
How to How to 12/17/2010
Products: WorkStation
Functionalities: Basic Functionality
Product version: 1.0, 1.1, 1.2, 1.3, 1.4, 1.5, 1.6, 1.7, 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022

Hiding the Search Bar

Hide the Main Menu if you do not use it or if you think it takes up to much space.

To hide the Seach bar
  • In WorkStation, on the Main Menu, click View, point to Toolbars, and

    then select Search bar.

(TaskClosing) The result of the task or information on which is the next procedure(s)

Community Content

Product version

Language