All licenses bought from a Schneider Electric vendor are delivered in an entitlement. The entitlements specify the products and features you are allowed to use.
For more information on how to order, contact your local EcoStruxure BMS vendor.
The entitlement ID is the designation that represents the license purchased by the customer. This ID is included in the entitlement that is sent by email when an order is approved.
The email with the entitlement also contains an HTML-file, the Entitlement Certificate File. This file is important when you add and set up the entitlement in Device Administrator.
Licenses for EcoStruxure Building Operation software and for field servers are delivered in entitlements.
License products for EcoStruxure Building Operation software are managed by License Administrator.
License products for field servers are managed by Device Administrator.
Mixed entitlements that contain licenses managed by Device Administrator and licenses managed by License Administrator. Device Administrator and Licenses Administrator has a built-in filter that only allows the correct administrator to manage the licenses. For example, when a mixed entitlement is added to Device Administrator, only the licenses in the mixed entitlement that is managed by Device Administrator is visible and can be used using Device Administrator.
You can add one or many entitlements to Device Administrator or License Administrator.
You can of course, at any time, buy a new entitlement with new products that you add to your site.
A product may contain one or many features. All products have an activation ID that is used then the product is activated.
The product may contain one or many licenses for a specific feature.
You have a site with five field servers. You want all field servers to use SNMP notification and you want all the users of the field servers to be able to create personal dashboards.
The order request process involves License Activation Server and License Server.
Number |
Description |
1 |
The Entitlement ID , which contains the licenses to activate, is entered into the License Administrator. |
2 |
The License Administrator sends the entitlement ID to the License Activation Server. |
3 |
The License Activation Server sends the order information to the License Administrator. |
Para obtener más información, consulte EcoStruxure Building Operation Software Licensing Workflow .
The order request process for field server licensing involves Device Administrator, License Activation Server, and the field server.
Number |
Description |
1 |
The Entitlement ID , which contains the licenses to activate, is entered into Device Administrator. |
2 |
Device Administrator sends the entitlement ID to License Activation Server. |
3 |
License Activation Server sends the order information to Device Administrator. |
Para obtener más información, consulte Field Server Licensing on Field Servers Connected to Internet Workflow .