Use the Basic tab to view the schedule status information and to configure the schedule.
Analog Schedule properties – Basic tab
Component |
Description |
Value |
Select the value associated with the event.
|
Previous transition time |
Displays the date and time the value most recently changed. |
Time since previous transition (min) |
Displays the amount of time in minutes that has elapsed since the value last changed, rounded to the next minute. |
Next transition value a |
Displays what the Value property will be when it next changes. |
Next transition time a |
Displays the date and time the value will change. |
Time to next transition (min) a |
Displays the amount of time in minutes before the value changes. |
Following transition value a |
Displays the subsequent value following the next transition value. |
Following transition time a |
Displays the subsequent date and time following the next transition time. |
Time to following transition (min) a |
Displays the amount of time in minutes before the value changes to the following transition value. |
Remove past events |
Select True to enable the system to delete events older than 72 hours.
|
Effective period |
Enter the range of time a schedule is in service.
|
Default value |
Select the value of the schedule when there are no events in effect.
|
Lead object |
Select a lead schedule to reference.
|