Use the Enterprise Server view to start and stop the Enterprise Server service and configure the ports of the Enterprise Server.
|
Component |
Description |
|
Status |
Displays the current status of the Enterprise Server Windows service. |
|
Start Service |
Click to start the Enterprise Server. |
|
Stop Service |
Click to stop the Enterprise Server. |
|
HTTP Port |
Type the port number that the Enterprise Server listens to when communicating through the Hypertext Transfer Protocol. |
|
HTTPS Port |
Type the port number that the Enterprise Server listens to when communicating through the Hypertext Transfer Protocol Secure. |
|
TCP Port |
Type the port number that the Enterprise Server listens to when communicating through the Transmitting Control Protocol. |
|
System |
Displays the system log. |
|
Path |
Displays the path to the folder where the Enterprise Server database and other objects created by the Enterprise Server or users are stored. |
|
A warning indicates that you entered a conflicting port number or that the service is stopping. |