Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
Use the Axis tab in WebStation to change the x-axis settings of a trend chart.
|
Component |
Description |
|
Time mode |
Select the time mode of the x-axis. |
|
Start time |
Enter the absolute start time when Time mode is configured to Absolute . This time is the leftmost point of the x-axis. For more information, see Configuring the X-axis with an Absolute Time Span . |
|
Time span |
Type the relative time span of the x-axis when Time mode is set to Relative . The rightmost point of the x axis is the current time. For more information, see Configuring the X-axis with a Relative Time Span . |
|
Show gridlines for X-axis |
Select True to show gridlines originating from the x axis scale. For more information, see Showing Trend Chart Grid Lines . |