Use the User Account properties dialog box to configure the properties of a user account.
Component |
Description |
![]() |
Click to create a new user profile. For more information, see Create Object Dialog – Naming the Object Page . |
![]() |
Click to edit a user profile. For more information, see Profile Properties . |
![]() |
Click to remove a user profile. |
Disabled |
Select True to disable the user account. |
Force password change |
Select True to force the user to change password after the initial logon. |
Password |
Type the password again. |
Confirm Password |
Type the password again.
|
Expires on |
Enter an expiration date and time for the user account. By default, there is no expiration date for the account. |
Password never expires |
Select True to disable password's expiration date. |
System of measurement |
Displays the system of measurement for the user account. |