earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: User Management
Product version: 3.2, 3.3, 2022
10/15/2020

User Account Properties

Use the User Account properties dialog box to configure the properties of a user account.

 
action_zoom_plus_stroke User account properties
Figure: User account properties

Table: User Account Properties

Component

Description

 
action_zoom_plus_stroke

Click to create a new user profile. For more information, see Create Object Dialog – Naming the Object Page .

 
action_zoom_plus_stroke

Click to edit a user profile. For more information, see Profile Properties .

 
action_zoom_plus_stroke

Click to remove a user profile.

Disabled

Select True to disable the user account.

Force password change

Select True to force the user to change password after the initial logon.

Password

Type the password again.

Confirm Password

Type the password again.

Expires on

Enter an expiration date and time for the user account. By default, there is no expiration date for the account.

Password never expires

Select True to disable password's expiration date.

System of measurement

Displays the system of measurement for the user account.

  • General Information Properties – Basic Tab
  • User Accounts and User Account Groups
  • Profile Properties