earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Localization
Product version: 7.0, 7.1
10/30/2025

Adding or Changing a Unit and Prefix for a Value

You define and change the unit and its prefix for a value to ensure that the value is correct calculated.

Show More
action_close

Numeric objects and some property types in EcoStruxure Building Operation support configurable units of measure. In certain object types, the unit is predefined and cannot be modified. The configured unit applies to the value stored in the server.

Unit Categories

All units belong to a unit category. A unit category represents a physical quantity. Examples include:

  • Power: W, VA, horsepower, Btu/h

  • Temperature: °C, °F

  • Pressure, Length, Flow, etc.

Measurement Systems

EcoStruxure Building Operation supports the following measurement systems:

  • International System of Units (Metric)

  • United States Customary Units (US)

Some units are identical across both systems (for example A, V, %, s), while others differ depending on regional usage (for example °C and °F).

Units in WorkStation and WebStation

As in Microsoft Windows (Auto in WebStation)

Values are displayed according to the Region settings of the operating system running WorkStation or WebStation.

If the server stores a value in °C but the client’s region uses US customary units, the value is shown in °F.

As Configured in Object

The value is displayed using the unit configured in the object. The client’s measurement system does not affect the presentation.

When this option is used, unit conversion exceptions are disabled.

International System of Units (Metric)

Values are displayed in SI units.

United States Customary Units (US)

Values are displayed in US customary units.

Note:

The measurement system affects only how values are displayed in WorkStation and WebStation. Stored server values are not changed.

Default units

Each unit category defines a default unit for each measurement system. If a value must be displayed using a different measurement system than the one used to store the value, the system uses the category’s default unit for the target measurement system.

The following table provides examples of default units:

Table: Default Units

Description

DefaultSI

DefaultUS

Absolute Humidity by Mass

kg/kg

lb/lb

Absolute voltage in dB

dBuV

dBuV

Voltage realtive to one millivolt in dB

dBmV

dBmV

Voltage realtive to one volt in dB

dBV

dBV

Acceleration

m/s 2

ft/s 2

Acidity or basicality of solution

pH

pH

Acoustic loudness in dB

dB(A)

dB(A)

Alcohol concentration

ABV

ABV

Ampere Square Hours

A 2 h

A 2 h

Angle

rad

deg

Angular momentum

J.s

J.s

Area

m 2

in 2

Brewing color measurement

EBC

EBC

Capacitance

F

F

Color

Color.Temperature

Color.Temperature

Compressibility

m 2 /N

m 2 /N

Concentration

/million

/million

Concentration of extract

DegreesPlato

DegreesPlato

Conductance

S

S

Conductivity

S/m

S/m

Corrosion Rate

m/yr

in/yr

Currency

currency 1

currency 1

Current

A

A

Current Density

A/m 2

A/m 2

Data transfer rate

bit/s

bit/s

Density

g/m 3

lb/in 3

Diffusivity

m 2 /s

ft 2 /s

Dipole Moment

debye

coulombmeter

Dynamic Viscosity

Pas

Pas

Electric charge

As

As

Electric Field Strength

V/m

V/m

Energy

J

Btu

Energy Apparent

VAh

VAh

Energy Density

J/m 3

J/m 3

Energy Efficiency

EER

EER

Energy Reactive

VArh

VArh

Enthalpy

J/kg

Btu/lb

Enthalpy Dry Air

J/kg_dry_air

Btu/lb_dry_air

Entropy

J/K

J/K

Flavor measurement

EBU

IBU

Flow

m 3 /s

ft 3 /min

Flow Rate Mass

g/s

lb/s

Force

N

lbf

Frequency

Hz

Hz

The density of all types types of paper

g/m 2

g/m 2

Heat Capacity

J/(g.C)

Btu/(lb.F)

Heat Degree Days

Cdays

Fdays

Heat Degree Hours

Chours

Fhours

Heat Degree Minutes

Cminutes

Fminutes

Heat Degree Seconds

Cseconds

Fseconds

Heat Flux

W/m 2

Btu/(s.ft 2 )

Heat Transfer Coefficient

W/(m 2 .K)

Btu/(s.ft 2 .K)

Humidity

% Rh

% Rh

Illuminance

lux

lux

Inductance

H

H

Length

m

ft

Linear Momentum

N.s

N.s

Luminance

cd/m 2

cd/m 2

Luminous efficiency

lm/W

lm/W

Luminous Flux

lm

lm

Luminous Intensity

cd

cd

Magnetic Dipole Moment

A.m 2

A.m 2

Magnetic Field Strength

A/m

A/m

Magnetic Flux

Wb

Wb

Magnetic Flux Density

T

T

Mass

g

lb

Mass Transfer Coefficient

(mol/(s. m2 ))/(mol/m 3 )

(mol/(s.ft 2 ))/(mol/ ft3 )

Mass Velocity

g/(s.m 2 )

lb/(s.ft 2 )

Mole Percent

mol%

mol%

Moles

mol

lbmol

Moment of Inertia

g/m 2

lb/ft 2

Momentum

g.m/s

lb.ft/s

NoCategory

NoUnit

NoUnit

Particle concentration

particles/m 3

particles/ft 3

Percentage

%

%

Percent Obscuration

%/m

%/ft

Phase

deg

deg

Power

W

Btu/s

Power Factor

cosf

cosf

Power Reactive

var

var

Pressure

Pa

psi

Pressure Drop Per Length

Pa/m

psi/ft

Pulsed Power Technology

pulse/min

pulse/min

Radiation absorbed dose

Gy

Gy

Radiation dose equivalent

Sv

rem

Radiation dose rate

Sv/h

rem/h

Radioactivity

Bq

Bq

Radioactivity Concentration

Bq/m 3

Ci/L

Relative density

SG

SG

Resistance

ohm

ohm

Resistivity

ohm.m

ohm.m

Seasonal Energy Efficiency

SEER

SEER

Site Specific Flow

volumetric_flow 1

volumetric_flow 1

Site Specific Volume

volume 1

volume 1

Site unit

site_unit 1

site_unit 1

Specific Entropy

J/(g.K)

Btu/(lb.R)

Specific Humidity

gH2O/kg_dry_air

grH2O/lb_dry_air

Specific Volume

m 3 /g

ft3/lb

Surface Energy Density

J/m 2

J/ft 2

Surface Tension

N/m

lbf/ft

Temperature

C

F

Temperature Diff

deltaC

deltaF

Temperature Rate of Change

C/min

F/min

Thermal Conductance

W/(m 2 .K)

W/( m2 .K)

Thermal Conductivity

W/(m 2 .K/m)

Btu/(h.ft 2 .F/ft)

Thermal Linear Expansion

m/C

in/F

Thermal Pressure

psi/F

psi/F

Thermal Volume Expansion

m 3 /C

in 3 /F

Thermoelectric Power

V/K

V/K

Time

s

s

Time Accuracy

s/h

s/h

Time per temperature

min/K

min/K

Torque

Nm

lbf.in

Turbidity

NTU

NTU

Velocity

m/s

ft/s

Velocity Angular

RPM

RPM

Voltage

V

V

Volt Square Hours

V 2 h

V 2 h

Volume

m 3

in 3

Unit Exceptions

You can define unit conversion exception rules when a unit other than the default unit is preferred.

For more information, see Adding a Unit Conversion Exception .

Other Exceptions

Values are always shown using the configured unit in the following contexts:

  • Alarms and trend logs in wizards

  • Customized alarm views

  • Alarm and trend log properties panes

Delta Temperature Conversion

The software converts units independently of context. To correctly convert delta temperature values, the unit must belong to the Temperature Diff category.

Absolute temperature conversions include both a multiplier and an offset, for example: T (°F) = T (°C) × 9/5 + 32

Delta temperature values must therefore use the following formula:ΔT (°F) = (9/5) × ΔT (°C)

For more information, see Delta Temperature Conversion .

To add or change a unit and prefix for a value
  1. In WorkStation, in the System Tree pane, select the value or point you want to configure.

  2. On the File menu, click Properties .

  3. In the Basic tab, click the Configuration button

     
    action_zoom_plus_stroke
    .

  4. In the Configuration tab, select Unit .

  5. In the Unit box, enter the unit.

  6. In the Prefix box, select the prefix of the unit.

  7. Click Select .

  8. In the Value dialog box, click OK .

  9. In the Properties dialog box, click OK .

  • Regional and Language Overview
  • Units
  • Metric Prefixes
  • Precision Format
  • Select Unit Dialog Box
  • WorkStation does not Display Correct Values