earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms, Basic Functionality, Schedules, Trends, User Management
Product version: 7.1
6/24/2026

Function Overview

arrow1_rotationRegional and Language Overview arrow1_rotationAlarm Overview arrow1_rotationSchedules Overview arrow1_rotationTrend Overview arrow1_rotationUser Account Management Overview arrow1_rotationBackup and Restore Overview arrow1_rotationDocuments Overview arrow1_rotationSearch Overview arrow1_rotationShortcuts Overview arrow1_rotationCloud Connectivity Overview arrow1_rotationExternal Log Storage Overview arrow1_rotationEnergy Consumption arrow1_rotationBilling Report

The EcoStruxure Building Operation software gives you a number of functions to monitor and manage your facilities.

Regional and Language Overview

WorkStation presents language, date, time, currency, unit, and decimals according to the user’s operating system settings.

For more information, see Regional and Language Overview .

Alarm Overview

You use an alarm to monitor a variable and to alert you if the monitored variable matches the configured alarm conditions.

For more information, see Alarms Overview .

Schedules Overview

A schedule is a sequence of events that determines when essential events occur in a building automation system: doors locking or unlocking, temperature raised or lowered, or equipment turned on or off.

For more information, see Schedules Overview .

Trend Overview

The function of a trend log is to log the variable that it is connected to and store the records.

For more information, see Trends Overview .

User Account Management Overview

When logging on to an EcoStruxure BMS server, you have to authenticate yourself by using a valid user account. The user account has to belong to the same domain as the server you log on to.

For more information, see User Account Management Overview .

Backup and Restore Overview

You backup your EcoStruxure BMS server data so that it can be restored after damage or loss due to hardware or software failures, security threats, or application testing.

For more information, see Backup and Restore Overview .

Documents Overview

A Document is a container in which you can upload (import) a file for use in the EcoStruxure Building Operation software. You can upload all types of files, including reports, forms, images, and video clips.

For more information, see Documents Overview .

Search Overview

Use Search in WorkStation to find and view objects in the database.

For more information, see Search Overview .

Shortcuts Overview

In the EcoStruxure Building Operation software, you can create shortcuts to objects in the System Tree pane. A shortcut is a link to a target EcoStruxure BMS server, folder, or other object and is simply a pointer to an object which acts as if it is that object.

For more information, see Shortcuts Overview .

Cloud Connectivity Overview

When cloud connectivity is enabled, the EcoStruxure BMS sends data from the system to the central storage for diagnostics and analysis along with data from other buildings and sites.

For more information, see Cloud Connectivity Overview .

External Log Storage Overview

You use External Log Storage feature to store historical data from EcoStruxure Building Management System (BMS). The amount of stored data is limited only by the equipment you use, and not by the capacities of the feature.

For more information, see External Log Storage Overview .

Energy Consumption

You can monitor, process, and analyze energy consumption using the consumption monitor, the consumption processor object, and the consumption signature object in EcoStruxure Building Operation.

For more information, see Energy Consumption Overview .

Billing Report

A billing report provides a detailed breakdown of a customer's electricity charges, consumption, demand, and associated costs for a specific period. It serves to show consumers how their energy usage translates into costs, verify utility bill details, and is often used in business settings to allocate energy expenses to specific departments or tenants. Key components typically include energy charges, fixed service fees, and taxes.

For more information, see Billing Report .

  • EcoStruxure Building Management Overview
  • Regional and Language Overview
  • Alarms Overview
  • Schedules Overview
  • Trends Overview
  • User Account Management Overview
  • Backup and Restore Overview
  • Documents Overview
  • Search Overview
  • Shortcuts Overview
  • Cloud Connectivity Overview
  • External Log Storage Overview
  • Energy Consumption Overview
  • Billing Report