Our site will be unavailable from October 29-30 due to scheduled maintenance.
Thank you for your patience.
The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management.
All modules connect to a hardware terminal base backplane. When the I/O module is installed on that terminal base, the EcoStruxure Building Operation software associates the I/O module with the position of the terminal base. There are a maximum of 32 positions per I/O bus that any terminal base can occupy.
For more information, see I/O Modules Overview .
The MP Series controller is an IP-enabled, native BACnet field controller from Schneider Electric. It is a highly flexible, open protocol device that is fully programmable through the EcoStruxure Building Operation software for control and supervision of equipment typically used in HVAC applications. Its mix of universal I/O and intelligent SmartX sensor support allows for a wide-range of control solutions.
For more information, see SmartX IP Controller - MP Series Overview .
The EcoStruxure BMS is a native BACnet system with features that enable you to create and manage an interoperable BACnet building automation system according to the ASHRAE Standard. The EcoStruxure BMS features and components support the BACnet services in all five of the BACnet interoperability areas.
For more information, see BACnet Overview .
b3 BACnet devices are a family of intelligent, programmable, stand-alone devices that provide Direct Digital Control of air handlers and systems as well as individual terminal units: VAV boxes, fan powered induction units, unit ventilators, and heat pumps.
For more information, see b3 BACnet Device Controllers .
MNB BACnet devices are a family of programmable, stand-alone devices that provide direct digital control in a building's environmental control system. MNB BACnet devices comprise MNB-70, MNB-300, MNB-V1, MNB-V2 and MNB-1000 devices. MNB devices support S-Link sensors, which are designed specifically for use with these devices.
For more information, see MNB BACnet Device Overview .
LonWorks is a fieldbus standard that is used for the automation of various functions within buildings, such as lighting and HVAC. The platform is built on an open, scalable protocol, called LonTalk that was developed by Echelon Corporation and supported by LonMark International.
For more information, see LonWorks Overview .
The Xenta 280/300/401 LonWorks devices are a family of programmable, stand-alone devices that provide Direct Digital Control of air handlers and systems as well as individual terminal units.
For more information, see Xenta LonWorks Device Overview .
MNL LonWorks devices are a family of programmable, stand-alone devices that provide direct digital control in a building's environmental control system. MNL LonWorks devices consist of standard MNL LonWorks devices and MNL-800 LonWorks devices. MNL devices are complemented by S-Link sensors, which are designed specifically for use with these devices.
For more information, see MNL LonWorks Device Overview .
Modbus is a master/slave protocol used for communicating with industrial hardware. The protocol works by one master device requesting data from (or writing data to) one or more slave devices.
For more information, see Modbus Overview .
I/NET is an integrated building management system that uses software and a mix of hardware to provide environmental control, access control, and energy management solutions. I/NET uses a proprietary, token-passing communication protocol, operating in a tiered LAN architecture.
For more information, see I/NET Overview .
The NETWORK 8000 system is a modular and integrated facility management system.
For more information, see NETWORK 8000 Overview .
MicroNet provides control of Heating, Ventilation, and Air Conditioning (HVAC) devices such as fan coil units, heat pumps, rooftop units, boilers, and air handling units
For more information, see MicroNet Overview .
Sigma is a building management system that comprises controller device and communications components which can be applied to a variety of environmental and building control services. The system components are seamlessly linked by a suite of user interface and control software called Satchwell Sigma.
For more information, see Sigma Overview .
Infinet devices are intelligent, programmable, stand-alone devices that provide cost-effective Direct Digital Control of air handlers and systems, as well as individual terminal units: VAV boxes, fan powered induction units, unit ventilators, and heat pumps. Using the EcoStruxure Building Operation software, you configure an Infinet network that connects WorkStation with SmartX AS-P servers and Infinet devices. Their true peer-to-peer communications protocol provides the Infinet series with the ability to instantly communicate with a SmartX AS-P server and its entire network of devices.
For more information, see Infinet Device Overview .
The SmartDriver functionality enables you to create customized interfaces in an EcoStruxure BMS that monitors and controls third-party devices from an EcoStruxure BMS server.
For more information, see SmartDrivers Overview .
Web Services are programmable applications accessible from standard Internet protocols. You can use Web Services to consume information, such as temperature from a weather service.
For more information, see Web Services Overview .