301 Topic(s)
You create an out of reference range alarm to trigger an alarm when a variable, such as a temperature, differs from a reference value.
You create an out of range alarm to trigger an alarm when a variable, such as a temperature, is not within its specified range.
You create a change of state alarm to trigger an alarm when a variable, such as a switch, is either true or false.
Trend log records substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the trend log records.
Use the notification workflow to create a notification including a notification report template.
Use the Configure Variable Triggered Notification page to create a variable triggered notification.
Use the Configure SNMP page to configure the SNMP properties of the notification.
Use the Configure Attachment page to set up the attachment you want to attach to the alarm.
Use the Assignment page to set the assignment conditions that have to be met for the alarm to be assigned.
Use the Attachment propertiesto edit attachments and configure whether or not the attachments are displayed when the alarm is triggered.