361 Topic(s)
Listed below are the System Alarms with IDs that begin with the letters E-L.
The EcoStruxure Building Operation software gives you a number of functions to monitor and manage your facilities.
You add an attachment, for example a .pdf file or trend log, to assist the user when diagnosing or solving the problem that caused an alarm.
You add an attachment, for example a .pdf file or a trend log, to assist the user when diagnosing or solving the problem that caused the alarm.
You configure an alarm to make a sound when it is triggered so that the operator can hear the alarm.
You configure the built-in Alarm pane to automatically open an Alarm View dialog box in a new window when an alarm is triggered.
You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.
You can customize how date and time are presented in a notification text or a notification report text.