earth_america
user_standard Log on
action_search_stroke
earth_america

Alarms

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

382 Topic(s)

How to

You create an out of reference range alarm to trigger an alarm when a variable, such as a temperature, differs from a reference value.

How to

You create an out of range alarm to trigger an alarm when a variable, such as a temperature, is not within its specified range.

How to

You create a change of state alarm to trigger an alarm when a variable, such as a switch, is either true or false.

Concept

Listed below are the System Alarms with IDs that begin with the letters E-L.

Concept

When an input, output or value in a connected device is configured to generate an alarm, Operator Display allows you to view and acknowledge the alarm. Inputs, outputs or values can be configured to generate an alarm when it is, for example, out of range or in a fault state.

Concept

SpaceLogic™ Operator Display is a touch-screen Human Machine Interface (HMI) for SpaceLogic controllers and servers, designed for local monitoring of building controllers in small and medium-sized buildings, as well as in large buildings with comprehensive building management systems. Operator Display is specifically designed for equipment rooms and it simplifies operations, service, and troubleshooting for System Integrators and Service Engineers, as well as for non-technical users (notably Facility Managers and Janitors).

Concept

Alarms substitution codes represent the information you want to display when a notification report is triggered. The information is dynamically filled in from the alarms that are included in the notification report.

Concept

The write to file notification is written to a text file or to an XLSX file when the configured notification condition is met.

Specifications

User Interface

Use the Alarm Control Panel Properties to view the referenced lead object.