89 Topic(s)
The SpaceLogic Bluetooth Adapter allows you to establish a Bluetooth connection to SpaceLogic and EasyLogic controller models. To connect to a device through the SpaceLogic Bluetooth Adapter, a SpaceLogic Sensor must be wired to the controller.
Running the Commission mobile application on a Windows laptop computer, you can connect directly to an Ethernet port on a networked BACnet/IP controller, or use an Ethernet switch to connect to a group of controllers.
You connect to the network and acquire an IP address so that you can communicate with the devices on that network. Most network connections used with the Commission mobile application assign an IP address to your mobile device using DHCP, which is a type of automatic addressing. However, certain Ethernet or WiFi networks may require you to use a static IP address. Consult with the network administrator to determine if a static IP address is required.
When connecting to a network at the job site, the Commission mobile application device must have either a dynamic or static IP address.
You log on to the Commission mobile application to perform commissioning, flow balance, and checkout operations on BACnet/IP controllers.
The Commission mobile application allows you to use a mobile device to perform commissioning, flow balance, and checkout operations on SpaceLogic BACnet/IP devices. BACnet/IP devices include BACnet/IP controllers (MP and RP), and IP-IO modules. The Commission mobile application is available for Android and iOS (Apple) phones and tablets, as well as devices using Microsoft Windows. The Commission mobile application can connect to a single BACnet/IP device or to a network of BACnet/IP devices on the local network.
Use the Device Restart function to perform a device restart of the BACnet/IP controller.
After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.
You connect to a device to begin all commissioning tasks.
You test the light outputs to ensure that DALI lights are operating correctly and are properly associated.