90 Topic(s)
You export an Asset list when you have completed the capture of controller data.
You can use the Asset List Creator feature to capture device information contained in the digital matrix symbol on the tear-off product information label packaged with the BACnet/IP controller. When you scan the data matrix with the Commission mobile application, the Asset List Creator saves this information to a data file that can be exported and used in documenting the physical location of the controller on the job site.
You can use the Asset List Creator function of the Commission mobile application to capture device information from the Digital Matrix symbol on the tear-off product info labels of BACnet/IP devices.
Use the Device Restart function to perform a device restart of the BACnet/IP controller.
You perform I/O checkout on the Multi-I/O module to verify that the devices are wired correctly and that the physical inputs and outputs are working properly.
Use this workflow to perform flow balancing on a single VAV controller, using the Commission mobile application. Related information can be found in the section after the flowchart.
Using the Commission mobile application, you flow balance a VAV unit at each designated setpoint to achieve the desired air flow.
After you have wired the physical inputs and outputs of the controller, you perform I/O checkout to verify that the wiring was done correctly and that the physical inputs and outputs are working properly.
You test the DALI relay outputs to ensure they are operating correctly.
You configure the VAV controller setpoints to set up the parameters by which the controller is flow balanced. These setpoints include the maximum flow setpoint, selected by default, and the intermediate and minimum flow setpoints, which are optional.