88 Topic(s)
SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.
You must configure the DIP switches as part of the commissioning process for the RP and MP controllers and RP-IO modules that only support BACnet MS/TP communications.
Use this workflow to commission one or more devices using the Zero Friction Commissioning function in the Commission mobile application. Related information can be found in the section after the flowchart.
The Commission mobile application provides the user with a means to generate a flow balance report that documents several values:
You can reset and restart the RP controllers in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.
You must configure a unique MS/TP address for the RP and MP controllers and RP-IO modules that only support MS/TP communications. You do so during installation by using position 1-7 on the address DIP switch.
In the Project List view of the Asset List Creator, you can view existing projects and delete or create new ones.
You can reset and restart the IP-IO and RP-IO modules in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.
You export an Asset list when you have completed the capture of controller data.
You can use the Asset List Creator feature to capture device information contained in the digital matrix symbol on the tear-off product information label packaged with the BACnet/IP controller. When you scan the data matrix with the Commission mobile application, the Asset List Creator saves this information to a data file that can be exported and used in documenting the physical location of the controller on the job site.