576 Topic(s)
You clear the list of the display names and IP addresses of servers when you do not need the contents anymore.
The Operating details dialog box displays more detailed information on what went wrong during the operation.
You log on to WorkStation to securely access the functions in the EcoStruxure BMS.
You edit a backup rule on an EcoStruxure BMS server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another EcoStruxure BMS server.
You configure the Archive settings and schedule on the Enterprise Server or Enterprise Central to automate the archiving process.
You back up multiple EcoStruxure BMS servers manually to copy and store data that is frequently updated.
All system events, as well as information and circumstances, are recorded in the Event log. These event records can be viewed in the Events pane or in an Event View.
You add a file extension to the Permitted File Extensions list so that EcoStruxure Building Operation users can open, save, and import files with that file extension.
Use the Building Operation WebStation window to log on to WebStation.