34 Topic(s)
In WorkStation, you add one or more Xenta OP operator panels to the Building Operation network.
Building Operation supports the major communication protocols in building automation and security management.
You print an I/O wiring list for the I/O bus that describes which I/O points are associated with each I/O module. You use the printed copy of this list to help wire the I/O bus network.
You print labels to identify I/O channels on the placard of an I/O module much the same way you label circuits on an electrical panel. You accept the default names for the I/O point labels or customize the I/O point names for your own application.
The I/O bus is a common bus that delivers power, address information, and communication to all devices connected to the bus. The I/O bus is provided to the devices through the backplane in the terminal bases. The term I/O bus also denotes the chain of devices that are connected together.
The I/O bus imposes restrictions on the number of devices that can be connected to the bus and what type of devices that are allowed on certain positions.
The I/O bus consists of the following parts: