earth_america
user_standard Log on
action_search_stroke
earth_america

Communication Configuration

Central IO
BACnet/IP devices
RP Controller Expansion Modules
SE8000/VT8000
Touchscreen Room Controller
In-Room Door Lock Gateway
ION
BACnet
LonWorks
Modbus
KNX
Zigbee
IoT
OPC UA
Web Services
SmartDrivers
Engage Mobile Application
RP-C-RC-BLE
Xenta
MNL
MNB
b3
Infinet
NETWORK 8000
I/NET
MicroNet
Sigma
Cloud Agent
Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

126 Topic(s)

Concept

The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management.

How to

You print an I/O wiring list for the I/O bus that describes which I/O points are associated with each I/O module. You use the printed copy of this list to help wire the I/O bus network.

How to

You print labels to identify I/O channels on the placard of an I/O module much the same way you label circuits on an electrical panel. You accept the default names for the I/O point labels or customize the I/O point names for your own application.

Concept

The I/O bus is a common bus that delivers power, address information, and communication to all devices connected to the bus. The term I/O bus also denotes the chain of devices that are connected together.

Concept

The I/O bus imposes restrictions on the number of devices that can be connected to the bus and what type of devices that are allowed on certain positions.

Concept

The I/O bus consists of the following parts:

Specifications

Specifications

Specifications

Specifications