108 Topic(s)
Use the Select Object dialog box to select the objects you want to add to the widget.
In the Point value widget and Log value widget, the units are normalized in such a way that entries with compatible units are normalized to the first listed unit in the category.
A search table widget is used when you want to display a Saved search as a widget in WebStation.
Use the Search Table widget dialog box to display a Saved search in a dashboard.
A point value is used to display the present value of one or many variables as a numerical value.
Use the Point Value Properties dialog box configure and edit a point value.
A log value displays one or many trend log values as numerical values.
Use the Log Value Properties dialog box to configure and edit a log value.
Dashboard widgets are small applications in a dashboard. Dashboard widgets are the main components in a dashboard and present graphical information from your system.
Dashboard Group Widgets is used to create a group of widgets inside a dashboard.