16 Topic(s)
You engineer your system using the engineering tools.
Use the Edit properties dialog box to edit the properties of objects connected to a graphic. The properties displayed in the Edit properties dialog box depend on the properties of the connected object.
Graphics can be added to a dashboard.
You scroll to move the graphic vertically or horizontally to see more of the graphic.
You use graphics to display building overviews, display values from sensors, or change setpoints. A graphic can also contain links to trend charts, trend log lists, Internet sites, or views in WorkStation and WebStation.
Use the object property dialog box to view or change the properties of a bound object. The link under each object opens a properties dialog box with a complete set of properties for that object.
Use the Graphics toolbar to navigate, zoom, and print a graphic.
You restore the graphic to its original size using Reset Zoom after you increased or decreased the size of the graphic.