Hardware

516 Topic(s)
Use the filters below to limit the number of search hits.
Products
Display all
WorkStation
WebStation
Graphics Editor
WebReports
Script Editor
Function Block Editor
Device Administrator
​License Server
​License Administrator
Software Administrator
Enterprise Server
PS-24V
AO-8
AO-V-8
DO-FA-12
DO-FC-8
UI-16
DI-16
UI-8/AO-4
UI-8/AO-V-4
UI-8/DO-FC-4
WebHelp
Automation Server
Administrator Tools
Power Supply
Central IO Modules
Project Configuration Server
Mobile Apps
Technician Tool for iOS
Technician Tool for Android
RTD-DI-16
Support Tools
Registration Portal
Transition
TAC Vista Conversion Tool
AS-P
AD v1
Project Configuration Tool
SmartXKiosk
Automation Servers
Continuum Conversion Tool
AS-B
Automation Server Smoke Control
AS-P Smoke Control
AD v2
MP-C
MP-V
Advanced Display
Enterprise Central
SpaceLogic Sensor
eCommission SmartX Controllers
BACnet/IP Devices
RP-C
IP-IO
AD v3
HMI Kiosk
RP-C-EXT-0-10V-4-PD
RP-C-EXT-BL-2-LV-PD
RP-C-EXT-BL-4-HV-PD
RP-C-EXT-DALI-M-PD
RP-C-EXT-MS-BLE
Engage
RP Controller Expansion Modules
MP-C Smoke Control
MP-V Smoke Control
IP-IO Smoke Control
RP-C-EXT-DALI
RP-C-EXT-0-10V-4
RP-C-EXT-BL-SMI-4-HV-PD
RP-C-EXT-BL-SMI-2-LV-PD
RP-C-EXT-REL-4
RP-C-RC-BLE
RP-C-EXT-KNX
Zigbee Adapter
CRS-HH-REL-10
Touch Screens
Operator Display
Builder for Function Block
Information Type
Display all
Concept
User Interface
Troubleshooting
Developers Reference
Specifications
How to
Hardware Installation
Topic
Modified
Rating
SpaceLogic Sensor Modular Bases and Covers
SpaceLogic Sensor devices are modular and are ordered in two parts: the sensor base and the cover. Four SpaceLogic communicating sensor base models are available as well as a variety of covers.
5/16/2022
Powering Up an AS-B Server
You perform the following steps to power up an AS-B server.
5/14/2022
Installing a Terminal Block on MP-C
You install the terminal blocks on the MP-C to add or enable wiring for the device.
5/13/2022
Installing a Terminal Block on MP-V
You install the terminal blocks on the MP-V to add or enable wiring for the device.
5/13/2022
Grounding and Power for Systems with RP-C-12A, -12B, or -12C Controllers
This section provides grounding and power recommendations for system configurations with the RP-C controller models RP-C-12A, -12B, or -12C, which are models that support 24 VAC/DC input power.
5/12/2022
MP-V Controllers
The MP-V controller is a multi-purpose, fully programmable, IP based field controller dedicated for VAV applications. MP-V integrates a controller, a damper actuator, and an air flow sensor in a single package for ease of installation. MP-V is a native SpaceLogic device, which can either be used as a standalone BACnet/IP field controller or as part of an EcoStruxure BMS with a AS-P or AS-B server, or an Enterprise Server, as the parent server.
5/6/2022
MP-V Damper Actuator
The MP-V has an integrated damper actuator, which allows for simplified installation of MP-V directly over the damper shaft.
5/6/2022
External Device Connections
There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.
5/5/2022
Moving the Damper Shaft Mounting Screws to the Alternative Positions on MP-V
You move the two damper shaft mounting screws to the alternative positions to be able to install the MP-V over a damper shaft with an exposed length that is less than 54 mm (2.125 inches) but greater than 22.2 mm (0.875 inch).
5/5/2022

Product version

Language