Use this workflow to activate licenses offline. Offline activation is typically used when Device Administrator and the automation servers are not connected to the Internet. Related information can be found in the sections after the flowchart.
All licenses bought from a Schneider Electric vendor are delivered in an entitlement. The entitlements specify the products and features you are allowed to use.
Use the License Information Enterprise Central dialog box to view the status of the licenses on the Enterprise Central or on the attached Enterprise servers.