56 Topic(s)
Consistent date and timestamping across a network is critical for system wide access control, security, communications, scheduling, alarms, and events. Network time uses the NTP protocol that provides the correct current UTC time.
Numeric objects and some property types in EcoStruxure Building Operation support configurable units of measure. In certain object types, the unit is predefined and cannot be modified. The configured unit applies to the value stored in the server.
Diagnostics in WebStation is a method of check the health of your system. Using Diagnostics you can also resolve several issues in the system, for example unconfigured trend log and forced values. You can check the following using diagnostics in WebStation:
You display the server time using a Time Stamp Value object when you want to display the local time for a server in another time zone than the client time zone.
Use the Time tab to configure the network time server addresses or establish a lead and shadow relationship on EcoStruxure BMS servers.
You define and change the unit and its prefix for a value to ensure that the value is correct calculated.
You add a language to WebStation so that the user can change to this language.
Use the Add or remove languages dialog box to add or remove language that can be selected in WebStation.
Use the Date and time tab to configure the server to use an external NTP server and to configure a time zone.
The EcoStruxure Building Operation software handles values and numbers with the highest precision. By default, the unit of a value is converted according to the regional settings of the user’s operating system.