48 Topic(s)
You view a graphical representation of your meter processor to better understand the energy consumption.
You reset a meter object, for example, after a testing. After the reset the meter object restart calculations and logging.
Meter objects can be reset. This is typically done after you have tested a meter object configuration or when you want to restart the calculation and logging in a meter object.
The meter object can take different status and modes.
The meter processor object is used to process the information from one or many meter objects. Using the meter processor, you can add or subtract energy consumption from many different meter objects. A meter processor can also process information from another meter processor.
The meter processor has a built-in mechanism to avoid negative consumption.
Use the Meter Processor Properties – Input dialog box to add and calculate values from a meter object or a meter processor to a meter processor.
Use the Meter Processor View to display and edit some properties of a meter object.
You can display a chart in WebStation that shows how much each connected meter object, or meter processor, contributes to the calculated result.
Use the Meter Processor– Outputs tab to view the output from the meter processor.