58 Topic(s)
When you replace a physical meter, you need to make adjustment to the meter object that monitor the physical meter.
Use the Consumption Signature – General tab to configure the consumption signature.
Use the Consumption Signature – Input consumption tab to add logs and edit logs.
You create a meter processor so that you can process and analyze the energy consumption.
You view a graphical representation of your meter processor to better understand the energy consumption.
Meter objects can be reset. This is typically done after you have tested a meter object configuration or when you want to restart the calculation and logging in a meter object.
You reset a meter object, for example, after a testing. After the reset the meter object restart calculations and logging.
You open diagnostics in WebStation to check the health of your system.
Use the Properties – Signature Coordinate dialog box to configure the coordinates for the signature curve.